Part Number: BQ25703A
Other Parts Discussed in Thread: BQ25703, BQ40Z50-R2
Hello,
first thanks for the great support as I have seen in other solved Questions. there are some Points that I want to make sure I rightly understood from the datasheet and some other General Questions.
- is there any available Signal from BQ25703 that indicate that charging is complete?
- OTG_Voltage and OTG_Current, are they a Limit for each or are they the value that the converter regulates resp. the OTG voltage and current at?
- can one send the following values to the microcontroller; inputvoltage, Inputcurrent, OTG voltage and OTG current, Vbat, Ibat from the Registers in the BQ25703? or should external circuitry be used. for example, one can connect pin 9 (IBAT) to the microcontroller but I would prefer to read it from the Register, is this possible and is there any difference in the readings?
- if I rightly understood, one can set the Input current Limit using the Ilim_HIZ pin. if this Limit it set through the Hardware, can one deactivate this Setting and set some other Setting through Software while hardwired Ilim_HIZ still connected?
Thank you very much.
Kind reagrds,
Amr