Part Number: REF3033
Hello all,
in my Design I use the REF3033 for Mikrocontroller ADC-Reference Voltage (VDDA33). There is a permanent minimum current of 3.3mA at "OUT"-Pin.
I also have an Analog Input Pin (Ana_IN1) at my µC. To protect the Ana_IN1, I connected a 7k68-Resistor in series. Also I connected a Diode from Ana_IN1 to the "OUT"-Pin of REF3033, so Overvoltage will not destroy my µC and current is limited. Normally there are about 2V at the Analog Input, but in case of a failure, there could be a higher voltage (12V and more) and so there will be more than 3,3V at the "OUT"-Pin of the REF3033.
Now my question is, what will happen with the REF3033 in case of a failure. What is the maximum external voltage/current at the "OUT"-Pin?
Thanks in advance
Best regards, Alex