This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54160A: TPS54160

Part Number: TPS54160A
Other Parts Discussed in Thread: TPS54160

Hi,

As per attached schematic diagram of TPS51460A data sheet, I have connected same rating components in In my hardware.

Voltage rating as per below-

I/P voltage- 48V

O/P voltage - 5V

O/P current - 1.5A

After frequency set,and set the load (around 1.5A),  In output I am receiving 5 V continuously. but after some delay around 01 minute I have seen that TPS54160A is heatup (at normal atmosphere its 100 degree C). 

Please support me, As 48 V input and 5V output, I have to change any component rating.

#heat #temperature #load #TPS54160 #datasheet 

Regards,

Ravi Jindal