Other Parts Discussed in Thread: EMB1428Q
Please advise,
I have em1402em controlled by external mcu. EMB1428 works fine with cell selection up to the moment when all switches are closed and EN signal goes high to 1.02V. From SPI CMD reply code for start balancing cell1 is 0x81: CS falling edge while the EMB1428 is still waiting for a transition on DONE (rising or falling edge).
on CMD 0x00 return code in previous frame is 0xA0 which says no error and shutting down instruction works fine.
After EN goes high value at EMB1499Q are:
EN = 1.02V
VSET = 1.8V
FAULT0 = 12V
FAULT1 = 12V
FAULT2 = 12V
DONE = 12V
CELPLUS to GNDF = 3.21V
VSENSE_HS to GNDF = 0V
VINF=PVINF to GNDF = 12V isolated
VINA=VINP to GND = 12V
It looks like EMB1499 stays in shutdown mode. And I can not figure it out why. All value stays in range. I have 3 boards and all 3 of them does the same.
Please help. Any advice will be helpful.