Hello.
When I turn on my device, the TPS3700 is set to a low level each time.
My scheme is attached to the message.
Q8 is de-soldered and wire-shorted.
Q14 is OFF. I also tried to de-solder it - no effect.
How to solve this problem?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
When I turn on my device, the TPS3700 is set to a low level each time.
My scheme is attached to the message.
Q8 is de-soldered and wire-shorted.
Q14 is OFF. I also tried to de-solder it - no effect.
How to solve this problem?
Hi StDenits,
Do you have scope shots of the circuit? They would help diagnose the issue.
Thanks,
Abhinav.
Hi StDenits,
I think isolating the device here to find the issue is the best course of action. As you mentioned, you tried disabling Q8 and Q14. I would then try to probe the nodes at your resistor divider outputs to see where we are still detecting an active voltage. The device seems to be detecting a low voltage. Also, why do you have an inductor connected on the Vdd line?
Thanks,
Abhinav,
@Abhinav.Sharma
>Also, why do you have an inductor connected on the Vdd line?
This is part of a 5V power filter.
It appears that the problem was the power sequence of the 5 V and 3.3 V DC voltage regulators. Small changes need to be made and power logic revise.
The TPS3700 works great in the case of UV (3.3 V -> 2.5 V): a high logic level is going low. Did not check OV, but should be the same.
That's my fault. Thanks for the help.