Part Number: TPS40210
Other Parts Discussed in Thread: LM5155
I am doing a design with TPS40210 with 15VIN(min), 19.2VINNOM), 22.8VIN(MAX) with VOUT = 24V IOUT = 3A. When I start a PMIC design I usually bring the equations into a CAS (Computer Algebra System) like MathCAD and use WebBench for a sanity check.
I don’t understand equation 22 in the TPS40210 datasheet and wonder if you could help me with that.
gM is conductance in units of siemens (S) alternatively A/V or 1/Ω but the equation doesn’t seem to match that and there is no background information on how the equation was arrived at.
In the numerator, we have product L x fSW this will result in impedance which divided by resistance ROUT and this becomes a unitless ratio. The denominator has ohms squared multiplied by the sum of a scaled resistance and another impedance. The units for the denominator is in resistance in ohms cubed.
There is an example, eq 59, in the datasheet that shows a result 19.2A/V (or 19.2S or 19.2 1/Ω).
The numerator solves to a unitless 0.020555 and the denominator as 1.071x10-3Ω3 .
This would make the solution 0.020555/1.071x10-3Ω3 or 19.2 1/ Ω3 (or 19.2 S3) and doesn't result in A/V as depicted in the datasheet.
Thanks,
Bob