Part Number: TPS54232
Other Parts Discussed in Thread: TPS54202
To TI Support Team,
as per TPS54232 datasheet device should work between input of 3.5V-28V.
I have implemented design using TPS54232 which should run on input range from 4V to 24V.
But at the input of 4V i am not able to get output of 3.3V @ 2A.
output is varying between 2.56 to 2.75V.
as per requirement design should work on 4V & 24V DC input.
is there any TPS54232 device constraint?
why i am facing this type of issue.
Please suggest.
Thanks,