This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62125: Hysteresis resistor calculations

Part Number: TPS62125

Hi,

I'm trying to implement the TPS62125 Enable Threshold and Hysteresis settings (EN and EN_hys pins). The datasheet Application section is clear about how resistors R_EN1 and R_EN2 affect the enable thresholds. However, there's very little information about how resistance at R_EN_HYS changes the hysteresis.

With a nominal VIN=12V and VOUT=5V, I chose these values:

VIN_startup = 10V
VIN_stop = 9V
R_EN1 = 1.1Mohm
R_EN2 = 147kohm
R_EN_HYS = 14.7kohm

How do I calculate the hysteresis in my design?

Thanks,
Michael