Other Parts Discussed in Thread: TPS546D24A,
I am using the TPS546D24AVEM and I am wondering how to control the output current? I have a 5V power supply connected to Vin and Ground In and then a programmable load. I know that I can adjust the output current draw by adjusting the load, but I was wondering if there is a setting in the Fusion Digital Tool Launcher to set what the output current should be like you can with the output voltage.
The main reason I ask this is because I can't seem to draw more than 5A. I am adjusting the load and getting between 0-5A, but no higher. Is 5A a limitation of this EVM?
Thanks