Other Parts Discussed in Thread: TPS63802
Hello,
I would like to ask if the VIN and VINA input must be the same, or is there any possibility to use lower voltage from voltage divider from VIN.
My idea is to use this IC with Li-Ion, and I would like to connect it to VIN a to VINA put 2 100K resistors. So if the battery would have about 3.4V the input voltage on VINA would be 1.7V.
Is this possible? Or do I need the same voltage for VIN and VINA?
Thanks
dbarvik