Other Parts Discussed in Thread: TPS55165-Q1, TMS570LS0432
I have a TPS55165-Q1 running on an TPS55165Q1-EVM Evaluation Module. After I set it up on the bench the converter was working correctly and it was powering the load correctly. I went through a few power cycles without issue. I then powered the device up and there was a 'pop' noise. Now there is no output voltage. I suspect the converter has failed somehow.
My setup is:
- The input voltage (VBAT on development board) was running off a lab PSU set to approx. 13.5 V.
- The output voltage selection jumper (J6) was set to 5V.
- The output voltage (VOUT) was being used to power a micro-controller development board (TI Hercules TMS570LS0432 LaunchPad).
- The PS jumper (J5) was in the PWM position.
- The PG_DLY (J4) jumper was not fitted.
- The SS_EN jumper (J3) was fitted.
- The IGN_PWR jumper (J2) was not fitted. Instead the IGN_PWRL was being controlled via the Hercules micro-controller (using a NPN transistor to drive the pin low to unlatch the supply).
- The IGN jumper (J1) was not fitted. Instead the IGN pin was wired to VBAT (13.5 V PSU) via a switch.
During the process of testing I was turning the lab PSU on and off several times. Usually I would start up VBAT with the IGN switch open, then after a moment closing the IGN switch to start up the converter. On the last time I powered up the device (when it failed) the IGN switch was already closed when I turned on the PSU. This might be coincidence or it may be related to the failure.
I see from the TPS55165Q1-EVM schematic that VBAT is filtered (VBAT_F) before it is is connected to VINP and VINL. With my bench setup, IGN is connected directly to the PSU (i.e. VBAT not VBAT_F). As VINP and VINL are filtered and IGN is not, then IGN could rise faster than VINP and VINL. Could this cause damage to the device? Is this the likely case of the failure? If IGN comes from a remote source do you recommend filtering or additional protection on the IGN input?
Thank you in advance of any help. Please let me know if you need more information to help diagnose the issue.