This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200-EP: VLDOIN Voltage Range

Part Number: TPS51200-EP

Good day. The datasheet for this part lists the VLDOIN Voltage Range in the feature bullet as 1.1 V to 3.5 V.

I'd like to use the part in an application with VLDOIN=0.95V and Vref=0.6V, in which supply current would be <500mA. According to the dropout curve (figure 14), this could work, but I don't know if there are regulation or stability problems it would incur. Any advice?