All,
Customer would like to use the output of the LM76002 (Vin= 24V) in an Oring configuration with 48V source. When the 48V is present the LM76002 will see 48V on the output and will turn off. Two questions.
Can the LM76002 withstand Vin =24V and Vout=48V continuously; I would think it should be fine but I could not see in the datasheet where it is discussed.
When the 48V is removed how long will it take the LM76002 to turn on and pass 24V to the output? Again could not find this in the datasheet.
Thanks,
Regards,
Joe