Part Number: LM25010
Other Parts Discussed in Thread: LMR14030
Hi all,
I'm looking for a pin-to-pin compatible device for the LM25010 which is able to support up to 2.4A of output current. Point is that it is not possible to modify the PCB for convenience while new requests are cooming for the specific voltage rail perfomances during board phase out. I'm allowed to modify sorrounding components.
Application is:
Vin=36V, Vout=24V, IoutMAX=2.5A.
the schematic is nothing different by the reference from the datasheet.
Can you help me?
Thanks!