Other Parts Discussed in Thread: LM5176
Using LM5175 for buck-boost converter. Switching frequency ~250KHz.
Only notice recently that when running boost mode: Input 12V, output 15V @ 20A, the top right FET (supposed to be syn FET) has no boot-strap gate drive: ie. the voltage of gate drive (pin19) is the same as the source voltage (pin18). So only the body diode conducts, FET does NOT turn-on and efficiency dropped. Checked boot-strap voltage on pin 20 and is normal, but no boot-strap at gate drive on pin19. Checked there is NO short-circuit gate-source on the FET in question.
When operating in buck-mode, boot-strap gate drives are normal on the relevant FETs.
Any experience/suggestion on this and can anyone help?