Other Parts Discussed in Thread: TPS543C20A
Hello
Can you Provide Reference Design for below Condition?
VIN : 8V ~ 14V
VOUT : 3.35V
IOUT : 25A
Temperature : 70℃
Switching Frequency : 500kHz
soft_start : 2ms
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Can you Provide Reference Design for below Condition?
VIN : 8V ~ 14V
VOUT : 3.35V
IOUT : 25A
Temperature : 70℃
Switching Frequency : 500kHz
soft_start : 2ms
Best Regards.
When simulating the TPS56221 in Webench, the temperature was high with criteria above.
I used the TPS543C20A in Webench to create the attached design.