I'd like to use the TPS54200 as a constant-voltage battery charger with variable current limit (microprocessor controlled via the PWM input). For example, could I set the output voltage to 7V using the FB pin to charge a 6V SLA battery and use the PWM input to limit current? (current limit would vary with battery size/capacity).