Other Parts Discussed in Thread: TPS55010, LM25017
Is it permissible to use TPS62175 for Fly-Buck? What are the features of implementation.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Alex,
I have never seen any applications using TPS62175 as a flybuck. Can you look at TPS55010? It is specifically intended for flybuck applications:
Thanks, John!
There is input voltage = 7..9V. Need to get two output = 5V/5V( or 3.3V/5V ), one is isolated. I wanted to use LM25017 (use it in another project), but Webench shows Vin_min=9V.
Thought I could use another synchronous buck as fly-buck.
Thanks!
I tried tps 62177 as Flybuck. Not so good. It goes to a lower switching frequency and creates a double key switch. There are waveforms.