hi. Respected engineers.
1. tps92511 is not a calculator document? Required.
2. Is low brightness control related to inductor value when analog dimming?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jay,
This device works well under Continuous Conduction Mode (CCM), i.e. the current regulation will not be accurate if it runs in Discontinuous Conduction Mode (DCM). Therefore, inductor selection is key if you would like to do analog dimming.
We do not have Excel calculator for this device. But the parametric calculations are easy (as you can find them all from the datasheet).
Switching frequency (in kHz) = 10 x 10^6 / RFS (while RFS is the resistor connected between FS pin and ground).
LED current (in A) = 1500 / RIADJ (while RIADJ is the resistor connected between IADJ and ground, max of 30 k-ohm).
And as above mentioned, inductor selection is important to make sure your full range of LED current output are running in CCM.
Thank you!