Hello
Our customer is applying TPS65262-2RHBR.
The applicable specifications are as follows.
VIN = 5 V
Voutput = Buck 1 / 3.3V, Buck 2 / 3.3V, Buck 3 / 1.5V
problem
1. Buck2 is Enable, but PWM output is 0V.
2. Buck3 is Enable, but 2.5V output.
Can you figure out where the two cases above can occur in the block diagram?
Please let me know what is expected.