Other Parts Discussed in Thread: TIDA-00652, DRV10983,
Hi
I have been experimenting with the reference design TIDA-00652 , I have seen few issue over period of testing . I am facing two issues.
1. The SMPS does not go in protection mode even if the draw on the output is over 30watts, so over 24Vdc at 1.25 AMP, I have checked the values of the resistors and R2,R3 and R6 have 1% variation in the values. Similarly R16 and R17 are 191K, with 1% variation.
2. The BaiseHV circuit has over heating issues and fries when the smps draw is over the specified values.
What may be the issue? there circuit is constructed using exactly the same components as in the BOM.
Thanks