This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56339: What will the output voltage be if the input voltage is lower?

Part Number: TPS56339

Hi,

I plan to use this chip to stabilize the output voltage at 12V. The input voltage can be between 11.5V to 14V. I want to know what the output voltage will be when I provide 12V/11.5V input voltage respectively? Can the high side MOSFET be always on so that I get output voltage = input voltage? 

Thanks, 

Xiaoming Wang