This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563209: Need Phase Margin and Gain Margin Simulations of TPS563209DDCR

Part Number: TPS563209


Hi Sirs,

My customer requests Phase Margin and Gain Margin simulations of the TPS563209DDCR device, while we don't see an option in the Webench utility.
Here we need product line's supporting in this case. We can send customer's information by Email.

Case #1: Vin = 12.8V, Vout = 5.2V, Iout = 1.1A
Case #2: Vin = 12.8V, Vout = 5.5V, Iout = 1.0A
Case #3: Vin = 12.8V, Vout = 1.4V, Iout = 1.2A

Thank you and Best regards,

Wayne Chen
02/20/2020