Other Parts Discussed in Thread: TPS62810-Q1
hi, I got a problem during the test of the demo board of the TPS62410Q1-EVM. When the power was turned on, I set two DC / DC outputs to 500mA at the same time
(one connected to a power resistor and the other connected to an electronic load. And set the input 3.8V, current limit 3A),the output waveform is shown in the following figure, is there any way to avoid this voltage drop? Thank you!