This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90910: Cannot Assign PWM3 and PWM4 with Fusion Digital Power Design GUI

Part Number: UCD90910
Other Parts Discussed in Thread: UCD90SEQ64EVM-650,

Hello,

I am using the UCD90SEQ64EVM-650 evaluation board with the 10-Rail Sequencer and System Health Monitor with 10-Fan Control and setting up the 10 fans in the Fusion Digital Power Designer GUI in the offline mode.  When I try to assign the PWMs for a fan to PWM3 (pin 42 - PWM3/GPI3) or PWM4 (pin 41 - PWM4/GPI4), the GUI pops up with the Fatal Program Error copied below and shuts down the program.

The GUI is fine if I assign either of these pins to a fan Tach. line or as a GPI, but it won't let me assign them as PWMs even though the data sheet for UCD90910 and the Pin Selector in the GUI shows that these two pins can be used for fan PWMs.  For reference, I would like these pins to both be set to 25KHz initially, which is within the frequency range for them, but I cannot get to the step to input the frequency because the program shuts down before I can add this.

Is there a bug in the GUI that is causing the Fatal Program Error when I try to assign fan PWMs to PWM3 and PWM4?  Do I need to set something else up beforehand to use these two pins as PWMs?

Thank you.

Overview
--------

Application: Fusion Digital Power Designer 7.2.1.0
Operating System: Microsoft Windows NT 6.2.9200.0
.NET Runtime: 4.0.30319.42000
Memory Used: 125.00 MB

Exception
---------

System.ArgumentOutOfRangeException: Index was out of range. Must be non-negative and less than the size of the collection.
Parameter name: index
   at System.ThrowHelper.ThrowArgumentOutOfRangeException(ExceptionArgument argument, ExceptionResource resource)
   at TIDP.WinForms.Apps.DPGUI.el.au()
   at TIDP.WinForms.Apps.DPGUI.el.a0()
   at TIDP.WinForms.Apps.DPGUI.el.az(Object A_0, EventArgs A_1)
   at System.EventHandler.Invoke(Object sender, EventArgs e)
   at DevExpress.XtraEditors.Repository.RepositoryItemRadioGroup.RaiseSelectedIndexChanged()
   at DevExpress.XtraEditors.RadioGroup.set_SelectedIndex(Int32 value)
   at TIDP.WinForms.Apps.DPGUI.el.ar(Object A_0, a A_1)
   at System.EventHandler`1.Invoke(Object sender, TEventArgs e)
   at TIDP.PMBus.Parts.UCD90XX.Controls.b.a(h A_0, h A_1)
   at TIDP.PMBus.Parts.UCD90XX.Controls.b.a(PinUse A_0)
   at TIDP.PMBus.Parts.UCD90XX.Controls.b.a(Object A_0, OpenLinkEventArgs A_1)
   at DevExpress.XtraEditors.Repository.RepositoryItemHyperLinkEdit.RaiseOpenLink(OpenLinkEventArgs e)
   at DevExpress.XtraEditors.HyperLinkEdit.ShowBrowser(Object linkValue)
   at DevExpress.XtraEditors.HyperLinkEdit.DoClick()
   at DevExpress.XtraEditors.HyperLinkEdit.OnClick(EventArgs e)
   at System.Windows.Forms.Control.WmMouseUp(Message& m, MouseButtons button, Int32 clicks)
   at System.Windows.Forms.Control.WndProc(Message& m)
   at DevExpress.Utils.Controls.ControlBase.WndProc(Message& m)
   at DevExpress.XtraEditors.TextEdit.WndProc(Message& msg)
   at System.Windows.Forms.Control.ControlNativeWindow.OnMessage(Message& m)
   at System.Windows.Forms.Control.ControlNativeWindow.WndProc(Message& m)
   at System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam)

Loaded Assemblies
-----------------

Accessibility
   Version: 4.0.0.0
   Info Version:
4.8.3752.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/Accessibility/v4.0_4.0.0.0__b03f5f7f11d50a3a/Accessibility.dll
   Public Key Token: B03F5F7F11D50A3A
Com.Muegel.Misc
   Version: 2.0.88.29979
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Com.Muegel.Misc.DLL
   Public Key Token:
Com.Muegel.WindowsApp.Win32API
   Version: 7.0.0.29979
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Com.Muegel.WindowsApp.Win32API.DLL
   Public Key Token:
DevExpress.Data.v6.2
   Version: 6.2.10.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.Data.v6.2.DLL
   Public Key Token: 79868B8147B5EAE4
DevExpress.Utils.v6.2
   Version: 6.2.10.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.Utils.v6.2.DLL
   Public Key Token: 79868B8147B5EAE4
DevExpress.XtraBars.v6.2
   Version: 6.2.10.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.XtraBars.v6.2.DLL
   Public Key Token: 79868B8147B5EAE4
DevExpress.XtraEditors.v6.2
   Version: 6.2.10.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.XtraEditors.v6.2.DLL
   Public Key Token: 79868B8147B5EAE4
DevExpress.XtraGrid.v6.2
   Version: 6.2.10.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.XtraGrid.v6.2.DLL
   Public Key Token: 79868B8147B5EAE4
DevExpress.XtraNavBar.v6.2
   Version: 6.2.10.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.XtraNavBar.v6.2.DLL
   Public Key Token: 79868B8147B5EAE4
DevExpress.XtraPrinting.v6.2
   Version: 6.2.10.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.XtraPrinting.v6.2.DLL
   Public Key Token: 79868B8147B5EAE4
DundasWinChart
   Version: 7.1.0.1810
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DundasWinChart.DLL
   Public Key Token: A4C03DCE5DB22406
Free.CommandLine
   Version: 2.0.88.29979
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Free.CommandLine.DLL
   Public Key Token:
Free.Misc
   Version: 2.0.88.29979
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Free.Misc.DLL
   Public Key Token:
Free.WinForms.Misc
   Version: 2.0.88.29980
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Free.WinForms.Misc.DLL
   Public Key Token:
Fusion Digital Power Designer
   Version: 7.2.1.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/Fusion Digital Power Designer.exe
   Public Key Token:
Microsoft.GeneratedCode
   Version: 1.0.0.0
   Info Version:
<empty>
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
   Public Key Token:
Microsoft.mshtml
   Version: 7.0.3300.0
   Info Version:
<empty>
   Location: file:///C:/Windows/assembly/GAC/Microsoft.mshtml/7.0.3300.0__b03f5f7f11d50a3a/Microsoft.mshtml.dll
   Public Key Token: B03F5F7F11D50A3A
Microsoft.VisualBasic
   Version: 10.0.0.0
   Info Version:
<empty>
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/Microsoft.VisualBasic/v4.0_10.0.0.0__b03f5f7f11d50a3a/Microsoft.VisualBasic.dll
   Public Key Token: B03F5F7F11D50A3A
mscorlib
   Version: 4.0.0.0
   Info Version:
4.8.4121.0
   Location: file:///C:/Windows/Microsoft.NET/Framework/v4.0.30319/mscorlib.dll
   Public Key Token: B77A5C561934E089
System
   Version: 4.0.0.0
   Info Version:
4.8.4001.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System/v4.0_4.0.0.0__b77a5c561934e089/System.dll
   Public Key Token: B77A5C561934E089
System.Configuration
   Version: 4.0.0.0
   Info Version:
4.8.3752.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Configuration/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Configuration.dll
   Public Key Token: B03F5F7F11D50A3A
System.Core
   Version: 4.0.0.0
   Info Version:
4.8.4121.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Core/v4.0_4.0.0.0__b77a5c561934e089/System.Core.dll
   Public Key Token: B77A5C561934E089
System.Data
   Version: 4.0.0.0
   Info Version:
4.8.4121.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_32/System.Data/v4.0_4.0.0.0__b77a5c561934e089/System.Data.dll
   Public Key Token: B77A5C561934E089
System.Data.DataSetExtensions
   Version: 4.0.0.0
   Info Version:
4.8.3752.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Data.DataSetExtensions/v4.0_4.0.0.0__b77a5c561934e089/System.Data.DataSetExtensions.dll
   Public Key Token: B77A5C561934E089
System.Drawing
   Version: 4.0.0.0
   Info Version:
4.8.3752.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Drawing/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
   Public Key Token: B03F5F7F11D50A3A
System.Numerics
   Version: 4.0.0.0
   Info Version:
4.8.3752.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Numerics/v4.0_4.0.0.0__b77a5c561934e089/System.Numerics.dll
   Public Key Token: B77A5C561934E089
System.Web
   Version: 4.0.0.0
   Info Version:
4.8.4075.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_32/System.Web/v4.0_4.0.0.0__b03f5f7f11d50a3a/System.Web.dll
   Public Key Token: B03F5F7F11D50A3A
System.Windows.Forms
   Version: 4.0.0.0
   Info Version:
4.8.4121.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Windows.Forms/v4.0_4.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
   Public Key Token: B77A5C561934E089
System.Xml
   Version: 4.0.0.0
   Info Version:
4.8.3752.0
   Location: file:///C:/Windows/Microsoft.Net/assembly/GAC_MSIL/System.Xml/v4.0_4.0.0.0__b77a5c561934e089/System.Xml.dll
   Public Key Token: B77A5C561934E089
TIDP.DevEx.Skin1
   Version: 1.0.0.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.DevEx.Skin1.DLL
   Public Key Token: 95FC6C5621878F0A
TIDP.I2C.DeviceGUI
   Version: 1.0.0.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.I2C.DeviceGUI.DLL
   Public Key Token:
TIDP.Misc
   Version: 7.0.0.20998
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.Misc.DLL
   Public Key Token:
TIDP.Net.ProxyPrefs
   Version: 1.4.0.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.Net.ProxyPrefs.DLL
   Public Key Token:
TIDP.PMBus
   Version: 7.0.0.42754
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.PMBus.DLL
   Public Key Token:
TIDP.PMBus.Design.TimeModel
   Version: 2.0.88.20999
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.PMBus.Design.TimeModel.DLL
   Public Key Token:
TIDP.PMBus.DeviceGUI.UCD3000
   Version: 7.0.0.42772
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.PMBus.DeviceGUI.UCD3000.DLL
   Public Key Token:
TIDP.PMBus.ParameterControls
   Version: 7.0.0.42768
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.PMBus.ParameterControls.DLL
   Public Key Token:
TIDP.PMBus.WinForms
   Version: 7.0.0.42771
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.PMBus.WinForms.DLL
   Public Key Token:
TIDP.SAA
   Version: 2.0.88.20999
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.SAA.DLL
   Public Key Token:
TIDP.SAA.WinForms.Misc
   Version: 2.0.88.41447
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.SAA.WinForms.Misc.DLL
   Public Key Token:
TIDP.WinForms.Apps.DPGUI
   Version: 7.0.0.42773
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Apps.DPGUI.DLL
   Public Key Token:
TIDP.WinForms.Apps.DPGUI.DPGUI1
   Version: 7.0.0.1637
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Apps.DPGUI.DPGUI1.DLL
   Public Key Token:
TIDP.WinForms.Apps.DPGUI.HelpCenter
   Version: 7.0.0.41447
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Apps.DPGUI.HelpCenter.DLL
   Public Key Token:
TIDP.WinForms.Dundas
   Version: 2.0.88.21000
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Dundas.DLL
   Public Key Token:
TIDP.WinForms.Misc
   Version: 2.0.88.41446
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Misc.DLL
   Public Key Token:
TIDP.WinForms.Util
   Version: 2.0.88.20999
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/TIDP.WinForms.Util.DLL
   Public Key Token:
XtraDataTempAssembly
   Version: 0.0.0.0
   Info Version:
<empty>
   Location: file:///C:/Program Files (x86)/Texas Instruments/Fusion Digital Power Designer/bin/DevExpress.Data.v6.2.dll
   Public Key Token: