Other Parts Discussed in Thread: LM25118
I am conducting an evaluation test using "LM25118 EVAL".
The input voltage is set to 10V and the output voltage is set to 12V.
The load resistance is 5Ω and the output current is set at 2.4A.
The required test specification is a procedure to start up the input power supply 10V with the load resistance connected in advance.
However, when energized, the output voltage does not reach 12V. The output voltage oscillates at 1 to 2V.
It cannot be used in such a state.
Can the "LM25118 EVAL" be used in this way?
Please tell me the correct usage.
Also, please let me know the method if it can be used by changing the component constants.
Thank you.