Other Parts Discussed in Thread: LM9061, LM5069, LM5066, LM5050-1-Q1, LM5060-Q1
Dear Sir,
I am using LM9061 for hotswap of two supplies from mains and Battery,to swap the Voltage of 24 Volt.
I am using two LM9061 to drive two mosfets.I am using Source pin of N Channel Mosfet as Battery Input and Drain Pin as Hotswap Output.
Enable signal we are getting from Micro controller.Drain Pin of mosfet is connected to VCC pin of LM9061.
Thresold pin of LM9061 is connected to Source and Sense Pin of LM9061 is Connected to Drain of the mosfet.
This IC can be used for this type of application.Please verify and Confirm.