Hi,
I have a requirement where I would like to use the TPS7A4001DGNR to generate the variable voltage from 85V to 90V based on my input voltage which can vary from 88V to 92V.
Is it possible to do the above variations with TPS7A4001DGNR?
If I set the Output voltage to 88V with R1(88.8K) and R2(1.2K) values, then If I provide 88V input what would be the response of the Regulator?
Please let me know ASAP.
Thanks & Regards,
Nanjunda M