Other Parts Discussed in Thread: GPCRA0, BQ40Z50
I was able to clear the CUV and CUVC alarms by reinstalling the firmware, CHEMID, and gg file I got back from the GPCRA0 tool. However, I now have a different issue, the charge cycle is terminated because an OC alarm trigger. I assume this is because my RSOC indication is constantly at 100%, even with a fully discharged battery. I have no idea why this is happening. I followed the instructions on your "BQ40Z50 Setup and Going to Production" video and I believe I have all my application setting correct. I have attached a copy of the gg file I got back from the GPCRA0 tool and a short log that shows hoe the charging cycle gets terminated only 3 minutes after it starts; this is with a fully discharged battery.
Thank you,
Jose Salazar8371.gg_out.csvCharge Test 2-26 2000 hrs.log.csv