Other Parts Discussed in Thread: TPS65131
I'm trying to use TPS63700 IC to produce ~-14 - 15 V output voltage. Depending on feedback devider I can produce output voltages down to ~-9V (under light or no load conditions). Any further decrease results in large current supplied from power source and output voltage close to -2V. A FB pin is no longer at ground level.
This is stable condition with PWM on state ~250 ns. Schematic used is shown below:
I've used 4.7 uH and 10 uH coils, and different feedback drivers - with no result. Also I've used feed-forward capacitor with RC conficguration as described in datasheet and in forums but with no result.
All other measurable signals are within normal parameters. I have had similar problem with TPS65131 negative voltage output with the same symptoms.
Sins this looks like problem with converter stability I'm attaching footprint below for reference:
All test I've decribed were made at light lodad or no load. I could use some advice what can cause this effects. This circuit should work with light loads with current consumption not larger than ~130 mA.