This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2672: Abnormal output voltage of LM2672MX-3.3/NOPB

Part Number: LM2672


Hi sir,

Regarding this part, at the moment a higher voltage 6V are output from  LM2672MX-3.3/NOPB when our production power on and repeating ON/OFF operation,

then the DP83822 in our production had a breakdown due to this reason.

Vin=24v DC

Please find the ripple below, yellow line is DC/DC converter output ripple, and aqua line is DC/DC converter input ripple.

Could you please help me to analysis why the output voltage is over 3.3V?

BOM:

L2:CLF10060NIT-470M (TDK)

    Max Vin:DC26V

    Max I:47μF/2A

   C52:GRM31CF10J107ZE01L (Murata)

    Max Vout:3.3V

    inductor: 100μF/6.3V

   D1:B240A-13-F (Diodes Incorporated)

    2A/40V

   C63:C2012X5R1V226M125AC (TDK)

    22μF/35V

   C51:GRM155B31H103KA88D (Murata)

    0.01μF/50V

  PCB layout design

   Vin:Red

   GND:Blue(Bottom to GND)

   Vout:Green

Best Regards,