This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54560B: About Output Voltage 28.8V. Duty 100% operation.

Part Number: TPS54560B
Other Parts Discussed in Thread: TPS54560EVM-515

Hello.

I have a question about TPS54560B.

Input: 40V-26.3V (stop sequence)
Output 28.8V 4A
Duty: Near 100%.
EN pin : 4V (higher than enable threshold voltage)
The HS-FET of TPS54560B  stop switching.
Why is this happening?
Thank you.