This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCH010505S: What's the output voltage accuracy of this part?

Part Number: DCH010505S

Hi team,

My customer is going to ues DCH010505SN7 in their design, and they're wonder what's the output voltage accuracy of this DCH010505SN7?

Please let me know if you have any ideas, thanks!

James

  • Hi James,

    The output voltage accuracy of the device is typical 10% within a 10 to 100% Load. I would recommend looking at Figure 3 in the datasheet.

    Note: When the device is operating below a 10% load operation, the device can be high as ~8V or slightly higher with 0 load. For applications that operate less than 10% of rated output current, it is recommended to add a minimum load to ensure the output voltage of the device is within the load regulation range.

    Regards,
    Alejandro