This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM33603EVM: No load current at 15mA

Part Number: LMZM33603EVM
Other Parts Discussed in Thread: LMZM33603

Customer is asking if LMZM33603EVM drawing 15mA in no load condition is normal?:

If I disable it, the current drawn is 650uA, which is expected, but in case of no load or light load, 15mA seems excessive. Please confirm if my reading is correct.

 Input: 18V

Output: 10V

Enable Hi

Current monitor on the input side. 14.5mA @ 18V

Thanks

Viktorija