Hello.
In the description in the data sheet,
The valid input voltage range of ISET is up to 0.8 V. With 10-mΩ sense resistor, the maximum output current is
4 A. With 20-mΩ sense resistor, the maximum output current is 2 A.
There is. From the following formula, is the maximum output current for a 40mΩ sense resistor correct at 1A?
Maximum charge current = 40mV ÷ Sense resistor
Please answer.
Please answer.