This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24316: Questions of triggering protection

Part Number: BQ24316


Hi,

About the device of BQ24316, I am confused about that if there is a surge, which is about 25V  peak , with a very short time, will it trigger BQ24316 to protect? I want know what is the minimum duration of the surge voltage that can trigger BQ24316 to protect? Which item is described in the datasheet?

I wish to get your reply. Thanks!

  • Hi Miles,

    The input OVP does not have a significant delay, see the BQ24316 data sheet tPD(OVP) parameter and figure 16.

    The battery does have a feature to ignore the surge, see the tDGL(BOVP) parameter.