Part Number: LM74670-Q1
Other Parts Discussed in Thread: TIDA-00858, CSD18532KCS, , LM74700-Q1, TLV1805
Hello,
I am designing a LLC resonant converter with output rated at 3.5kW/ 28V. Since the current drawn from load is around 120A, even the rectifier stage with SiC Schottky diodes causes a lot of conduction losses and makes the converter efficiency really poor.
I came across LM74670 to use MOSFETs as smart diodes and find it very interesting. I looked into TIDA-00858 reference design and planning to test out similar design to see if it fits with the customer requirement.
I have a couple of questions and would be awesome if you can clarify these:
1. Do you think the Full bridge rectifier technology can be used in resonant converter (like LLC) secondary stage to rectify square waves signals? My switching frequency is around 150 kHz. I am just planning to use them as just for rectification stage without any smart-logic. Do you see any potential problem with this?
2. My load current is around 120A, hence I think the MOSFETs (CSD18532KCS) used in TIDA-00858 will not cause thermal problems (ofc with good heatsink combination). Do you agree with this or should I look for MOSFETs with higher current rating. Awesome would be if you can recommend me something with very low Rds,on that is good compatible with the IC. What additional recommendation you suggest to the ref design to accommodate high current.
3. Do you have any literature to calculate conduction losses in such Smart diodes in bridge configuration? Some clarification or hints on that would be nice.
Thank you and looking froward to hear from you.
Regards,
Sidd
P.s We hope you and yours are staying healthy and this corona situation will be over soon.