Other Parts Discussed in Thread: LM2574, LM2674, LM2675, LM22675
Hello,
I'm considering to use a TL2575 for a application with the following values:
Vin = 24V
Vout = 5V
Iout = 375mA
From the Graph on the datasheet (Figure 14) it the inductor should be 680uH.
Can you please clarify if i only have to take into account the maximum current?
I'm asking because the 375mA is the peak current but it normal functioning it can be lower and as such i wanted to make sure that it would work properly( lets say if nominal Iout = 200mA or less ).
Thank you.