Other Parts Discussed in Thread: TIDA-01573, LMG1020, SN65LVDS4, DS90LV028A
Hi Team,
The datasheet of the LMG1025-Q1 specifies a VIH High Threshold voltage of 1.7V (min) and 2.6V (max). Does this mean that any voltage between 1.7V and 2.6V will be interpreted as a "High" input, or does this parameter specify part-to-part variation in the VIH?
Another related question is about what happens when the VIH applied to the IN+/- pins is higher than 2.6V? My customer is using an LVDS driver with a 2.4V min and 3.1V Typ output voltgae. Could this damage the inputs of the LMG1025-Q1?
Thanks and Regards,
Mihir