Part Number: UCC21222-Q1
Hi Team,
I could see the propagation delay (min 28ns and max 40ns) is given for 0 load capacitance.
I'm trying to measure the same with mosfet mounted.
Do we have a curve with propagation delay vs load capacitance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCC21222-Q1
Hi Team,
I could see the propagation delay (min 28ns and max 40ns) is given for 0 load capacitance.
I'm trying to measure the same with mosfet mounted.
Do we have a curve with propagation delay vs load capacitance.
Mohana,
Thanks for your question.
You are correct that this parameter its not specified in the datasheet, only for 0pF load.
We can use the PSPICE model can be used to estimate or simulate the delay over load capacitance.
This is located in the product folder here:
For example, i simulated the prop delay at several load capacitance, up to a very extreme value using the sample project provided as part of our PSPICE model for UCC21222-Q1. The results are below, as well as a quick snap of the design file we provide. Please note that this is uses the typical model at a fixed temperature, and should be used for estimation.

I hope this helps you. If this answers your question, please let me know by clicking the green button. And let us know if you have any additional questions.
Best
Dimitri
Hi dimitri,
Thanks for your response. It resolved my issue. I will try out with the simulation.