Other Parts Discussed in Thread: TPS54360, PMP10088
Hi,
I'm currently designing around the TPS54160A to create +/-12V +/-300mA and referencing the application note SLVA369A as well as the Reference Design for the PMP10088 (which uses TPS54360). I've set the switching frequency to be 300kHz. In the reference design schematic Rev B version for the PMP10088, an RC snubber is added across D1. Is this necessary to include for the TPS54160A and if so, can you please help with tuning the values for the RC snubber?
Can you please review my schematic below:
Thanks!