Other Parts Discussed in Thread: BQSTUDIO, , BQ27520-G4
TI 技术支持您好,我已经准备好BQStudio 以及 EVM的环境,正在进行下一步的学习,有几个问题想咨询一下您:
Hi TI technical support, I have prepared the BQStudio and EVM environment, and are learning the next step. I have a few questions to ask you:
问题一:BQ27520EVM 开发版的PACK+ 、PACK- (连接充电器的 + 、 - )允许的输入电压范围是 2.7~4.3 ,但是我们的电池充电电压必须在4.4V 才能充满。 我能否调整CHARGE的电压4.4V 接入EVM?
Question 1: The allowable input voltage range of PACK + and PACK- (+,-connected to the charger) of the BQ27520EVM development version is 2.7 ~ 4.3, but our battery charging voltage must be 4.4V to be fully charged. Can I adjust the voltage of CHARGE to 4.4V to access EVM?
问题2:关于学习周期目前我有两份文档,一份是BQStudio的SLUA903–July 2018 Achieving The Successful Learning Cycle 。 另外在BQ27520EVM开发版的 Users Guide 中也有关于学习周期的内容。 然而,经过我的研究,我发现两份文档的描述有不同点 ,我应该参照哪一份?
Question 2: Now I have two documents about the learning cycle. One is SLUA903–July 2018 Achieving The Successful Learning Cycle by BQStudio. In addition, there is a content about the learning cycle in the Users Guide of the BQ27520EVM development board. However, after my research, I found that the descriptions of the two documents have little different. Which one should I refer to?
问题3: 我倾向于按照文档SLUA903–July 2018 Achieving The Successful Learning Cycle 中的步骤进行学习周期。 在第一个环节我就碰到了问题,在5页的最底下,文档中的描述如下:
Question 3: I tend to follow the steps in the document SLUA903–July 2018 Achieving The Successful Learning Cycle. I encountered a problem in the first link. At the bottom of the five pages, the description in the document is as follows:
Q1: Does the battery have to be full before starting the first link
Q2: When I click the IT_ENABLE button in BQStudio. Update Status flag is not set
Q3: Is there a big impact if the CHEM ID is not specified? Did it cause Q2?