Hi all,
I’m using the BQ24075TRGTT and all appears to be working correctly except that CHG pin is always low (charging). I have confirmed that the CHG pin / tracking is not shorted to any other signal.
My circuit is a below and any suggestions would be as appreciated.
IN = 4.7V CE = 0V
R1 = 24k (3 hours) SYSOFF = 0V
R2 = 3.9k (0.4A) EN1 = 0V
R3 = 5.76k (0.155A) EN2 = 3.3V
R6 = 20k TS = 0.92V
R7 = 8.45k VBat = 4.12v (battery connected)
The disconnected battery voltage is 4.11V
Many thanks...