Part Number: LP3905
Other Parts Discussed in Thread: LP3907
Hi Team,
In LP3905 datasheet has specify that :
Bucks outputs range: 1.0~3.3V and LDOs ouput range: 1.5V to 3.3V. with note (1)
(1) Fixed output voltage devices can be customized to fit system package. requirements.
Here need your help to see if we have available device or any limit to supply the LP3905 with the spec for 3.3Vin and two Bucks: 1.2V_0.45A and 1.6V_0.45A / one LDO 1.8V_50mA?
Best regards,
Albert Lee.