Dear Ladies and Gentlemen,
I have a pcb according to your design, but found out that the LMZ12008 is not outputting the 5 Volts requested, but a lot less voltage.
I used tried the following resistor configurations without luck:
R_ffb=1k89; R_fbt=10 k (calculation based on datasheet)
R_ffb=1k; R_fbt=7 k (calculation based on webench (approximate values)
The EN-pin is driven to 3.3 V by a microcontroller.
I tried the setting both with a 470n on SS as well as without the cap.
The input and output caps are designed as per datasheet requirements.
Also I noticed the voltage on the feedback pin not rising sufficiently when trying to get the 5 volt setting.
I prepared two configurations along with measurements under the link below:
1. R_ffb=1k; R_fbt=7 k (should output 5v but only outputting about 2 V)
2. Feedback to output, without voltage divider to get the minimum voltage
(The output was loaded with a 220 Ohms resistor)
https://postimg.cc/gallery/DXV0ycx
Could you please give me some hints why this problem occurs to me?
Thanks advance.
Kind regards