This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24750: Estimating runtime in varying (temperature) conditions

Part Number: BQ24750
Other Parts Discussed in Thread: BQ40Z80, BQ34Z100-G1

Is any of the SMBus enabled chargers able to give a (more or less accurate) estimate on the remaining battery capacity taking into account the current temperature?

Our system is going to be used in various environments from -20 to +65 °C.

It is my understanding that the SMBus command AtRateTimeToEmpty() only takes into account a hypothetical current value but there is no way for the battery itself to calculate the temperature into that. Are chargers available that can do just that?