Hello,
I'm using a CSD16301Q2 to drive a simple Laser. I chose the CSD163 because I wanted voltage controlled MOSFET to drive the gate from a GPIO on my CC2640r2. The gate voltage when turned on is 3.0VDC with the battery providing 4.5VDC. With the gate pulled to 3VDC I expect that the CSD163 will pass up to 20mA (limited by the 220 ohm series resistor). When I apply 4.5 volts to the laser with a bench power supply, it draws 11.8mA. Please have a look at my implementation shown below and let me know what I'm doing wrong.
Thanks,
Patrick