This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ23605: About latch-up

Part Number: LMZ23605

Hi,

I ask you about the latch-up of the LMZ23605.
This device has passed the latch-up test under the conditions specified in JESD78.

Question 1
If current or voltage stress exceeding the conditions specified in JESD78 is applied to the device, are there any measures to prevent destruction?
Please let me know if there is a document that describes latch-up measures.

Question 2
For example, under the condition of VIN = 0V and VOUT = 5V, will the device be destroyed?

Best regards,