Hi team,
Our customer will use TPSM53602 with the below condition
- Input voltage : 15V or 24V
- Output voltage : 6.8V
Here is the inquiries from them.
- Configuration of UVLO.
- Should customer configure that UVLO is about 10V since output voltage is 6.8V considering light load condition to avoid the output voltage ripple ?
- What is the purpose of R4 in the EVM ?
- In the datasheet, RFBT should be 10kohm as recommendation but the value in the EVM is different. Please give us the reason why there is the gap for datasheet.
- In the EVM, R1 is 402k ohm and the value is different from the datasheet which recommend 100k ohm.
Please give us the reason.
Thank you and best regards,
Michiaki