Other Parts Discussed in Thread: TPSM53603, , TPSM82822, TPS82085
Hi team,
I get a WEBENCH alert at following configuration:
Vin 4.1V -5.5V
Vout 1.2V (or 1.1V)
Iout 1A
WEBENCH Power Designer reports:The TPSM53602 device may not be stable when operating under PFM Mode
With Iout = 2A: I get the WEBENCH message that the design cannot be created:
Your preferred device does not work with the inputs you selected.
This design is not stable due phase margin either smaller than 35 or greater than 120.
But according to the data sheet, this configuration should work, right?
(With TPSM53603 I get the same messages)
Best Regards